A Shunt Trip w/ Communications is available on Stored Energy MTZ devices when System Communications have been selected. The Shunt Trip w/ Communications remotely trips the device by way of a communications network.

When a "Spring Charging Motor w/ Comms" is selected for this device then this "Shunt Trip w/ Communications" option shall automatically be selected with the default Voltage Rating of 120Vac.

 

Only 3 voltage systems are available. The Voltage must match the Closing Coil w/ Communications voltage.

 

Control Power is not supplied by Schneider Electric for the Spring Charging Motor, Shunt Trip / w Communications and Closing Coil w Communciations.

 

If this Stored Energy Device is a Main or Tie and part of an Auto Transfer Scheme then a "Shunt Trip w/ Communications" is not selectable.

.

  • Available Voltages available are indicated by "Y"
Rated Voltage- MTZ -
250Vdc 
125VdcY
48Vdc 
24VdcY
12Vdc 
6Vdc 
600Vac 
480Vac 
380Vac 
277Vac 
240Vac 
208Vac 
120VacY